This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH0397: Behavior of LMH0397 at No Power Input

Part Number: LMH0397

Dear Sirs,

My customer asked us about behavior of LMH0397 at No Power Input.

1.If an external HD-SDI signal is input while the LMH0397 is in the No power Input state, does the LMH0397 fail?

 By the way, his circuit is the same connection as "LMH0397 Typical Application Circuit" in the data sheet.
 The HD-SDI signal is input to the "SDI_IO +/-" pin.

And he has one more question.

2.Will the LMH0397 fail if it operates with the supply voltage below 2.5V?
  For example, when the power supply voltage is 1.2V to 2.0V.

Please let me know above questions.

Best Regards,

Y.Hasebe