Hi TI team
I found an issue for accessing UB953 failed.
The reproduced rate is about 1%.
Before that, I init UB954 successfully,
and then read DEVICE_STS(Address 0x04) is 0xDF (that means device LOCK and PASS status),
and then wait 300ms.
Could you kindly help to analysis this issue?
I think accessing UB953 will be successful after read DEVICE_STS LOCK and PASS status.
Is the waiting time not long enough?