Part Number: SN75DP130
Hi team,
The customer is considering using SN75DP130 as DisplayPort Redriver IC with the 5.4Gbps 4lane specification.
I have a question about the specification of IC,
1, Is it possible to replace and use P / N of each lane of input / output?
2, Is it possible to switch lanes (IN: 0, 1, 2, 3 → OUT: 3, 2, 1, 0) with input and output?
Also, are there any other suitable parts?
Thanks
Best regards,
Shidara