Part Number: TUSB8020B-Q1
Other Parts Discussed in Thread: TUSB8041
Hi
1: At present, TUSB8020B-Q1 achieves system-side power supply by system-side, not by USB. Just use the HUB function of basic USB 3.0.
Does the I2C interface of this chip need to be connected? Or is it just floating?
2: PWRCTL pin and OVERCUR1z pin power switch function and over-current protection function I do not need here, is it possible to connect pull-down resistance?
3.Because I don't have external USB, so I don't have 5V voltage when external USB is inserted. So, do I just look for a 5V voltage in the board and use the voltage divider resistance to connect the VBUS_DETECT_TMS pin?
4. This reset pin needs a pull-up resistor for power-up reset, but the pull-up resistor is not added in the user manual. Why is this? If pull-up resistance is needed, what is the recommended resistance value (ground capacitance is 1uf?)
5: I don't quite understand the use of PWRCTL_POL/SS_DN1 pin in the picture below. Can you explain it more specifically?
6. What does the POWER SWITCHING refer to below?
7. I saw the SMBus address settings, but I didn't see the I2C mode chip address settings.
Thank you
Jerry