This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90LV004: DS90LV004

Part Number: DS90LV004

Dear Sir,

  Customer asked the Sub-LVDS re-driver for 720P resolution display in DLP application.

  Q1: Due to the customer PCB layout needs a 10 inches in length, a re-driver is considered.

  Q2: Do you have P/N suggestion to us? 

  Q3: If there no part suggestion, may I use the LVDS RX/TX ( 2 devices ) to replace the Sub-LVDS re-driver?   

   Function Block is shown as below.

   www.google.com.ph/search

 

  • Hello,

    Just to confirm the requirements, you need buffers that will take sub-LVDS input and produce sub-LVDS output, right? If that's the case, we don't have any such buffers, unfortunately. Using LVDS RX/TX won't work either, since we don't have a LVDS driver that outputs sub-LVDS.

    Regards,
    Yaser