Hi,
I'm using this part in order to connect a massive storage device to a cpu.
During the loading of the firmware, using SPI, I noticed on the Input to the chip the signal has a masive undershoot, and only undershoot, no overshoot.
It gets to about -0.8 to -1 V. can it harm the part, is it outside the AMR? What can be the cause of this. the SPI is connected directly to the EEPROM.
Thanks.