Part Number: TPS65987D
Other Parts Discussed in Thread: TPS65983B
Hello
if customer would like Intel thoundbolt 3 , PD 65W, are TPS65987D or TPS65983B suitable solution? Thank you.
BR
Patrick
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Eric,
2 more questions about TPS65983 FW.
Hi Peter,
1. Yes, intel has a tool that will take the Full flash image from the 83B and the FW from the ridge and merge it into one image that can be programmed onto the shared SPI Flash.
2. Yes, intel has a tool for this as well. I would suggest asking them for more information on it.
Thanks,
Eric