This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB320: Specs Enable Pin

Part Number: TUSB320

In the datasheet under "Pin Configuration and Functions" (p.3) it is written:

EN_N
Enable signal; active low. Pulled up to VDD internally to disable the TUSB320L device. If
controlled externally, must be held low at least for 50 ms after VDD has reached its valid
voltage level.
EN —
Enable signal; active high. Pulled down to GND internally to disable the TUSB320H device. If
controlled externally, must be held low at least for 50 ms after VDD has reached its valid
voltage level.

Is it correct, that the Enable signal must be held low at least for 50 ms with the TUSB320L (active low) and the TUSB320H (active high)?