Part Number: SN65LV1224B
Other Parts Discussed in Thread: SN65LV1023A, SCAN921226H, SCAN921224
Good day folks,
We have an application where LVDS data is being supplied by a device that we cannot command to send Sync data. Up until it went EOL we had been using DS92LV1212AMSAX/NOPB Deserializer with complete success. When that went away we tried the recommended SN65LV1224BDB. We were not able to get LOCK to stick (our Deserializer won't stay locked if it does momentarily acquire lock) . The recovered rate is 264 Mbps (so we are supplying a 22 MHz Ref Clock).
We tried various other Deserializers and none seem to work. We have tried adjusting the Ref Clock (using more precise sources, etc.) but to no avail. As I mentioned above, we do not have the option to force the data source device to issue a Sync sequence so we must rely on the Deserializer locking with the random data method. I read on this forum that one of the nice things about the "old" 1212 was that it could accept a clock with a 5% tolerance whereas the new parts need something like +/-100 ppm.
Is there any part option available today that has that wider tolerance on the Ref Clock it accepts and can operate with that 22 MHz clock? If one of the Enhanced Performance devices would work, we would be willing to use that.
Many thanks, and best!
Eric