This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB7320: some question on TUSB7320

Part Number: TUSB7320

Hi Sirs,

Sorry to bother you.

Please help review of the TUSB7320I as below.

The other issues are as follows:
1. Is SCL/SDA not directly pulled down?
2. Does Power 3.3V and 1V have the order of switches?
3. As shown in the block diagram on the first page, my source is PCI host. How does TUSB7320I's WAKE# / CLKREQ# connect? WAKE#  Pull high / CLKREQ#  Pull down?
4. When do I need to use EEPROM? Isn't the preset correct?
5. Is there any special attention to Layout? Please also provide a Layout guide.

Thank you.