Part Number: TPS65987D
Other Parts Discussed in Thread: TIDA-01620, TUSB1064, TPS65981,
Hi, community member.
I want to make a board just like TIDA-01620, conversion from USB-C to DisplayPort.
But, it is difficult for me to develop software for MSP430 micro-contollers, because I'm not software engineer.
If I use TSUB1064 and TSP65987D, Can I make a USB-C to DisplayPort board without software as below ?
1. Main devices: TUSB1064, TSP65987D, SPI-FLASH
2.Make a binary file with tool "TPS65981_2_6_7_8 Application Customization 5.13". and write to SPI-FLASH.
New project / template type: standard / Upstream Facing Port only / Super Speed controller : None (DisplayPort only)
Edit Configuration Mode TAB, especially GPIO for matching with schematic.
If you say, I will need more process and settings to contol this board by firmware, I have to change my idea.
The purpose of this board is only internal use, not for production.
Input : USB-C / Output: DisplaytPort (UFP only)
Power Delivery: 5V 1.5A for supplying to these devices by 3.3V
Maximum resolution: 4k 60p or FHD 144kHz
Now I don't have these devides or evaluation boards.
I want to decide to start or give up this project by this answer.
Best regards