Part Number: SN75DP159
Hello,
I use this component of TI: SN75DP159
I'm looking at the datasheet on the Vsadj Resistor 7.06-kΩ where written:
"For the SNx5DP159RGZ:
Pin Strapping
HDMI2.0 & HDMI1.4b
Vsadj Resistor = 7.06-kΩ"
I want to know if it's critical for the Vsadj Resistor to be 7.06-kΩ or it can be also 6.98k / 7.15k ohm?
The reason I'm asking is because I need this resistor to be 0201 package and I can't find 7.06k ohm resistor for 0201 package.
Thank you very much,
Edan