This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65LVDS049: IBIS model reports errors

Part Number: SN65LVDS049


http://www.ti.com/lit/mo/sllc163/sllc163.ibs

I'm trying to use the IBIS model above in Hyperlynx SI VX.2.3_Update2 .  I've copied the data from the link into an .ibs file but when I go to assign the model, I get several errors:

C:\Projects\PVRPS\30kW_BACKPLANE\5022-9806\Current\PCB\Output\SN65LVDS049.ibs:
Success : Parse succeeded on file C:/Projects/PVRPS/30kW_BACKPLANE/5022-9806/Current/PCB/Output/sprm638a.ibs.
Warning : at line 937 in file C:/Projects/PVRPS/30kW_BACKPLANE/5022-9806/Current/PCB/Output/SN65LVDS049.ibs : Messages for model DRIVER_OUT:
;; Warning: The sum of the maximum clamp curves and the pulldown curve is not monotonic at voltage 3.5.
Error : �
Error : at line 1676 in file C:/Projects/PVRPS/30kW_BACKPLANE/5022-9806/Current/PCB/Output/SN65LVDS049.ibs : syntax error, unexpected IdentToken, expecting $end
Error : Parse failed on file C:/Projects/PVRPS/30kW_BACKPLANE/5022-9806/Current/PCB/Output/SN65LVDS049.ibs.

 

Anyone know how to fix this?  Thanks.