Part Number: DS90UB954-Q1EVM
Other Parts Discussed in Thread: DS90UB929-Q1, DS90UB940-Q1, DS90UB949-Q1
Hi,
This is regarding the DS90UB953/954 serializer/deserializer pair.
Can we connect the 954 to 933/913A also? Are they compatible?
Also, regarding the MIPI CSI 2 input interface to the 953, is it compatible with any MIPI CSI 2 Tx source?
Are there any specific parameters on the MIPI CSI 2 Tx that should match to the 953? like the data types ( RAW,RGB etc. ), or the pixel modes, or the virtual channels etc.?
Do we have any HDMI to FPD-Link III solution that is directly compatible with the 954?
Thanks and Regards,
Archit Adwant