This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB949-Q1EVM: USB2ANY (.hex) compile code to reprogram MSP430 in EVM

Part Number: DS90UB949-Q1EVM
Other Parts Discussed in Thread: USB2ANY, ALP

Hello TI community,

We are working with the DS90UB949-Q1EVM and currently we want to flash a test code on the MSP430 that is in the EVM  but at the end of the test we want to reflash the original code (USB2ANY) of the EVM's MSP430. Could you please share the USB2ANY (.hex) file in order to reflash the MSP?  


Note: we do not want the source code therefore we don´t want to modify the USB2ANY code. 

Regards.

Francisco Gomez

  • Hello Francisco,

    Please install the latest ALP-PROFILE-UPDATE (v05) from the following link

    http://www.ti.com/tool/ALP

    You can then find the hex file under the following folder
    C:\Program Files (x86)\Texas Instruments\Analog LaunchPAD v1.57.0010\Drivers\i2c_controllers\usb2any\Firmware

    Please note ALP Framework is version v1.57.0010. ALP-PROFILE-UPDATE are applicable for this latest framework version only. In case you are still on an older version, please install the framework v1.57.0010 and then the latest ALP-PROFILE-UPDATE patch.

    Thanks,
    Vishy