Part Number: TCA6424A
Other Parts Discussed in Thread: MSP-EXP430G2ET,
Hello...I am evaluating the TCA6424A for use as an LED driver in a new design. I am trying to get the IO Expander EVM and host MSP430 LaunchPad to work. I noticed that I have a Rev 1.0 MSP-EXP430G2ET LaunchPad which is different than the Rev 1.5 shown in the IO Expander EVM instruction guide. Still, I think I identified the jumpers that needed to be changed from their default settings: I switched the UART jumpers and removed the P1.6 jumper. I put the two boards together and connected the USB port to my PC. I ran the IO Expander Flasher.bat file and it fails to find a USB FET. It then finishes with an Exit 11 code, failing to load the 430.
Can anyone tell me if the Rev 1.0 LaunchPad is compatible with the IO Expander EVM? Any other ideas on why this isn't working? Thanks for any help...Mike