Part Number: PCA9545A
Hi team,
my customer want to use the PCA9545 as below:
So please help to answer below questions:
1. What's the Vpass voltage?
2. So in the application, it seems the Vpass need to be lower than 1.8V, so I need to refer to the typical value, then the VCC should be less than 3V right?
But if I want to have a margin, how should I choose the VCC? it seems the 3V is just point to 1.8V Vpass.
3. For the max and min, what's the indicated temperature? Does the max refer to high temp?
Lacey
Thanks a lot!