Hi,
My customer is evaluating the DP83867 and have a question.
According to the datasheet, the default value of RGMII_TX_CLK_DELAY(BIT[1]) is "0b0" on the RGMII Control Register (RGMIICTL), Address 0x0032.
And the default value of RGMII_TX_DELAY_CTRL(BIT[7:4] is "0b0111" on the RGMII Delay Control Register (RGMIIDCTL), Address 0x0086.
However they confirmed on the board that these default values changes depending on LED_1 pin and LED_2 pin setting.
The below attached file is the result they observed.
DP83867IRRGZ_register default value.xlsx
They assumed following from the results.
・The default value of RGMIICTL(Address 0x0032) BIT[1] is "0b0" in the case of RGMII Clock Skew TX[2:0]="0b100"(TX CLOCK SKEW=0ns), it is "0b1" in the case of except 0b100.
・The default value of RGMIIDCTL(Address 0x0086) BIT[7:4] is "0b1111" in the case of RGMII Clock Skew TX[2:0] ="0b100"(TX CLOCK SKEW=0ns).
In the case of except "0b1111", it depends on TGMII TX CLOCK SKEW.
e.g.) It is "0b1001 in the case of RGMII Clock Skew TX[2:0]="0bx111".
Are these assumption correct?
If yes, are these described on the datasheet?
Please let me know if you have any question.
Best Regards,
Kuramochi