Part Number: DS90UB953-Q1
Other Parts Discussed in Thread: ALP
Hi,
Would you please help clarify for me the clocking scheme/flexibility using 953/954. To better target your reply a brief explanation of our setup
-We are investigating a prototype design using the 954/953 FPD link chipset.
-We are operating in Synchronous Mode - no external oscillator on the 953 side of FPD link.
-The 954 has a 25MHz oscillator input to its REFCLK pin.
-We want to investigate the different performance - especially with regard to reach - when running Forward Channel at lower data rates
-We change the BCC rate using 954 register 0x58.
-We are using the Analog LaunchPAD to control the system
I want to understand what flexibility this setup provides in selecting the 953 Forward Channel Data Rate the 953 CLKOUT Frequency
It would be very helpful if you could answer the following questions:
1. The ALP information page returns a value of 23/24Mhz for the ‘Refclk Freq’. This is confirmed by reading Register 0xA5. Is this the 954’s approximate interpretation of the REFCLK input?
2. Is the back channel data rate directly controlled as an integer multiple/divider of the REFCLK? 50Mbps 2x REFCLK, 25Mbps 1x REFCLK, 12.5Mbps REFCLK /2 etc?
3. When the port status of the link is in ‘Pass’ state the ALP information page shows the ‘Linked’ speed as 2 times the BCC rate. To what speed is this referring?
4. Table 6 of the datasheet indicates how the FC data rate is calculated. For synchronous this is stated as ‘f x 160’. What is ‘f’’? Is it the same as the value given in the ‘REF FREQUENCY (MHz)’ column. Is it the frequency of the REFCLK at the 954? Is it determined by the BCC data rate?
5. Is it possible to set the Forward Channel Data Rate to either 4Gbps or 2Gbps with appropriate register settings? If so, what registers support this?
6. Once the Forward Data Channel Rate has been set there looks to be plenty of flexibility for setting the CLKOUT frequency.
7. Is there an App Note which could help clarify how the clocking domains are connected and controlled?
Thanks
Paul