Part Number: DP83867IS
Hello,
There is a note on page 94 that said "Keep traces as short as possible; less than 2 inches is recommended with less than 6 inches as maximum length" for the RGMII.
One of our customers has a main board that uses 7 inches and by the time it gets to the PHY on their daughter board there is another 2 inches. So there is a total of 9 inches maximum.
I'm hoping the guidelines are conservative. The customer's previous PHY from a competitor allows 15 inches maximum for RGMII trace lengths. Can we make this work?
Thank you,
Ryan B.