This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH0074: CLC014 alternative with lower transfer rate

Part Number: LMH0074

Hello,

There is an application note CLC012 replace to LMH0074 but LMH0074 supports >=125Mbps. We are using 80Mbps by CLC014. This is out of LMH0074 spec.

Is there any good solution tof adaptive equalizer to support 80Mbps?

Best regards,

Toshihiro Watanabe

  • Greetings Watanabe-San,

    LMH0074 is the lowest video rate equalizer that exist in the market. The reason you see 125Mbps typical minimum data rate is because this is a very popular rate in SDI industry. Please note 125Mbps is in typical column and thus I believe device is able to operate at 80Mbps. Also, you can enable bypass at such a low rate like 80Mbps.

    Regards,,nasser