Dear Sir.
I need ask 925+ 926 FPD-LINK III signal several questions.
1. What is the 35-bits of the Forward Channel transmission? Is 24 DIN[23:0] + 4 sync signals + 2 I2C + 3 I2S audio = 33 bit?
2. What are the Back Channel transmissions bit?
3. Is the Forward Channel and Back Channel transmitted simultaneously at the FPD-LINK III signal? Is there a more detailed timing diagram explanation?