This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDS171RGZEVM: Jumper for I2C_EN PIN (J3)

Guru 19785 points
Part Number: TMDS171RGZEVM
Other Parts Discussed in Thread: TMDS171

Hi Team,

Looking at the TMDS171/181 EVMs, I couldn't find the jumper for I2C_EN Pin (J3) by default.

Isn't this pin a LVCMOS input which requires high or low ? Does it have internal pull up or pull down ?

I also found a typo in the User's Guide (SLLU217A).

When I2C_EN PIN = Low (JP2-3), the device is only in PIN mode which I2C access can not be used.

This description in the manual is explanation for the J3, not for  the jumper setting JP2-3.

This sentence may confuse user, so could you please make modification in the next revision ?

Best Regards,
Kawai