Part Number: SN65HVD1781
Other Parts Discussed in Thread: SN65HVD1786,
I have a question regarding RS485 transceivers and voltage rating. On one of our interfaces we are running standard RS485 communication but also applying 12-16V when not communicating (driver disabled). The duty cycle is approximately 50%, so this is not something that happens occasionally. Currently we are using SN65HVD1786 for this specific interface:
Both input voltage and differential input voltage is within range when apply 16V.
SN65HVD1786 is a 5V part, but having a 3.3V part would make interfacing to 3.3V logic easier. We are looking at SN65HVD1781 and run with 3.3V supply, but then we will no longer operat withing recommended operation conditions:
However 16V is still within absolute maximum ratings:
Is it safe to operate in the area between recommended operating conditions and absolute maximum ratings?
Will it limit the component expected liftime in any way and/or stress the component?