Part Number: TUSB4041I
Other Parts Discussed in Thread: TUSB8041
Tool/software: Linux
Hi
We have a TUSB4041 mounted on our Jetson TX2 carrier board to split out the Jetson's USB2.0 upstream port to four USB2.0 downstream.
The Jetson is running Ubuntu 16.04
Using lsusb -vvv Ubuntu reports:
Bus 001 Device 002: ID 0451:8142 Texas Instruments, Inc. TUSB8041 4-Port Hub
and
SuperSpeed USB Device Capability:
bLength 10
bDescriptorType 16
bDevCapabilityType 3
bmAttributes 0x00
wSpeedsSupported 0x000e
Device can operate at Full Speed (12Mbps)
Device can operate at High Speed (480Mbps)
Device can operate at SuperSpeed (5Gbps)
The TUSB4041 is clearly not a Super speed device, however per the datasheet its VID:PID are 0451:8142, which is identical to the VID:PID in the TUSB8041's datasheet.
Is this intentional? Is the TUSB8041 Super speed driver for Ubuntu untended to be backward compatible with the TUSB4041?
We have tested various devices with the hub. Mass storage devices successfully connect at USB2.0, however our XIMEA USB2.0 is not recognised at all.
Strangely, if we connect an additional standalone hub to one of the TUSB4041's downstream ports, the camera connects.
Could this be related to Ubuntu loading the 'wrong' driver?