Part Number: SN65DP159
Hello,
There is the following description in the register map of the datasheet.
"When changing crossover point , need to toggle PD_EN or external HPD_SNK" in DEV_FUNC_MODE field.
What does it mean?
I am using the fixed value which is the default setting. (2b01)
In this case, after changing input signal of SN65DP159 from VGA to FHD(Over 1Gbps), do I need to toggle PD_EN?
Best Regards,
Masaaki