This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB320LAI: pull-up resistor for ID pin

Guru 29720 points

Part Number: TUSB320LAI

Hi Team,

My customer is designing their system with TUSB320LAI for DRP application.
The datasheet shows ID pin should be pulled up to VDD using 200kΩ resistor as the following.



What is occured if 100kΩ or 1MΩ resistor is used for pull-up?
The background of the question is OTG USB controller has internal pull-up resistor that can be selected 100kΩ or 1MΩ.

Best Regards,
Yaita