Part Number: TCA9509
Other Parts Discussed in Thread: TCA9517,
Is the input voltage 1/0 threshold of this device fixed at a voltage, or at a percentage of the VccA/VccB? Our application uses relatively long I2C signal lines that may pick up some noise, and if the threshold is Vcc-based, I will use a full 5 volts on the far side to get the maximum noise immunity. If it is a fixed threshold, I'll probably use something like the TCA9517 instead, with 3.3V on both sides.