This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65987D: Possible to change Event Mapping of GPIO via on the default firmware with some simple I2C commands?

Part Number: TPS65987D

Hi

We would like to use the TPS65987D without flash since the default firmware (with Configuration 3 on ADCIN1) does all we need. The only thing missing is that we would like to map the "Cable Orientation Event" to one of the GPIOs, which doesn't seem to be mapped in the default configuration.

Is there a simple way to just configure the event mapping via I2C or would I need to generate a whole FW Image and load it into RAM (we use a simple MCU for all power management, which might not have enough flash to store a 16k binary)?

Thanks,

Mark