Part Number: TCAN1042HGV
Dear Team,
Is TCAN1042HGV can P2P replace MAX13052ASA+T?
Or only SN65HVD1050D can replace it?
BR
Kevin
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCAN1042HGV
Dear Team,
Is TCAN1042HGV can P2P replace MAX13052ASA+T?
Or only SN65HVD1050D can replace it?
BR
Kevin
Kuan,
If the customer needs the slope control on the Rs pin, the TCAN1042 does not have this or the SPLIT pin. However, slope control and the SPLIT pin are typically used to help with EM emissions, and the TCAN1042 was designed with emissions as a focus. The TCAN1042 can pass EM emissions without the need of the voltage stabilization from the SPLIT pin or the slope control of the Rs pin.
The TCAN1042 can indeed replace the MAX13052.
Regards,