Part Number: DS110DF410
Hi Team,
Q1). What is the REG 0x31 [4:3] setting ? These bits are set to "00" by default.
Q2). Is the default setting of REG 0x31 [4:3] correct ?
I also found the similar setting for DFE in REG 0x2C [5:4], which is set to "11" instead of "00".
Best Regards,
Kawai