Part Number: TUSB546EVM
Other Parts Discussed in Thread: TPS65982
Dear all
I have one TUSB546EVM, and I take Apple adapter to power on, as below picture,but there is not 20V output on the J13 connector
My questions:
1. How to set the EVM,so that my EVM can be output 20V on the J13 ?
2. Is the apple adapter fit to use with the EVM ? If not, Please recommend the adapter .
Thanks a lot.