Part Number: DS90UB933-Q1
Hi Sir
So far we meet DS90UB933 + DS90UB934 unlock issue for 10bit mode
1. May I know how to set 100MHZ for BIST mode ,I saw 0xb3[2:1] = 01 can use for 100MHZ ,but actually the output only 50MHz
2. In BIST mode when we set 0xb3[2:1] = 00 ,I think the clock source is from PCLK ,May I know PCLK can support 99MHZ ,Due to this condition 934 can't lock
3. 0x05 = 14 ,may I know bit 0 need to set 1 ?
4. 0x0C = 00 ,is it correct ?
5. 0x14 = 00 ,if I need to do 100Mhz BIST mode ,Do I need to change the value from 00 to 01 ?
6. Have anything can be take care to solve this issue ?
Unlock issue will happen on CMOS communication with SOC