Part Number: TIOL111
In TIOL111 application diagram it was mentioned that IO LInk device has Sensor, microcontroller, TIOL111 and then M12 Connector based on this can i use TIVA C Series 123gh6pm as a contoller with Temperature Sensor interfaced to TIOL111.
I contacted TMG regarding IO link Stack and Software before that i want to clarify the following doubts
1. Will i get the Temperature value from M12 Connector.
2. How we will set the parameter data(Status like Sensor health, power consumption ) which can be viewed on Computer when connected via Master
3. Which pin in TIOL111 takes care of parameter data transfer and how it is transferred?