This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB964-Q1: Very-rarely-happen issue with abnormal I2C log

Part Number: DS90UB964-Q1

I'm writing question on behalf of my customer.

This telematics system uses 3 cameras(913 ser) and 964 des.

During tens of thousand on/off test, customer founds no display signal issue. After restart, the symtom is gone and never duplicated again.

Comparing normal log, there're two abnormal logs of I2C communication.

1. Normal: /usr/bin/ccidbgr  /dev/v4l-subdev9 0x3d read 0x24

0x24 <- 0x00

Abnormal: /usr/bin/ccidbgr  /dev/v4l-subdev9 0x3d read 0x24

0x24 <- 0x24

CSI TX1 interrupt even though TX1 is not being used.

2. Normal: /usr/bin/ccidbgr  /dev/v4l-subdev9 0x3d read 0x4D

0x4d <- 0x43

 Abnormal: /usr/bin/ccidbgr  /dev/v4l-subdev9 0x3d read 0x4D

0x4d <- 0xC3

This RX port is not selected, but it is read.

 

This symptom is under investigation, but not easy to replicate. Please advise if there's something need to check. Thank you.