Hi community member.
I am thinking of converting USB-C to DisplayPort.
Could you tell me because I am in trouble about the descriptions in the user guide?
The schematic of Figure 6 described in the 10G-EXPANSION-EVM user guide shows the pin functions as follows:
4 SN_SSRX_P
5 SN_SSRX_N
7 SNK_SSTX_P
8 SNK_SSTX_N
The data sheet of the TUSB1064 alone is described as follows.
4 SSRX_N
5 SSRX_P
7 SSTX_N
8 SSRX_P
●Question
・P and N are reversed in the two documents.
Is the description of the TUSB1064 data sheet of the IC alone correct among the two documents?
・Is the following correct in order to make the two documents consistent?
Swap 4 and 5 in the 10G-EXPANSION-EVM user guide, and swap 7 and 8
Best Regards.