Part Number: XIO2001
Tool/software: Linux
Hi team,
I have questions about the meaning of registers as below on XIO2001 PCI bridge device. Would you please verify them below?
1. ANFEM bit (Reg:114h, bit13) :
This value of register depends on the occurrence of system booting issue. (Issued = "1b", non-issue="0b").
Customer inquires whether the corresponding register value changes according to which element of a system.
When I looked into the datasheet, this bit looks depending on the device reset. That is, this bit will be cleared after device reset normally.
so, if this bit is not clear, I think device reset is not performed normally. Am I correct? Is there any reason to be active this bit?
2. ANFES bit (Reg:110h, bit13) & UR_ERROR bit (Reg 104h, bit20)
When reading these registers(ANFES & UR_ERROR0, both bits are always active regardless of system booting issue.
We want to know the reason why these bits are active even though it's an error stats report. (It's not related to device issue but want to know the meaning exactly)
So, my question is that the conditions under which the error bit of the corresponding register values are marked and how the XIO2001 operation will change accordingly.
Thank you for your support in advance.
B.R
Tony