This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB2077A: Designing a 10 Port USB Hub

Part Number: TUSB2077A


Hello,

I wanna design a 10-port USB Hub. Maximum I can find is a 7 port Hub. So How I can I achieve it?

Thanks

Vishal Kakade

  • Hi Vishal,

    It is possible to tier hubs to get support for 10 ports.  In this case you could add a 4 port hub to one of the downstream ports of the TUSB2077A, so there are 6 exposed ports from the TUSB2077A plus 4 from the other hub.  Please be aware that the TUSB2077A supports operation only up to 12 Mbs, not USB high speed (480 Mbps).

    Regards,

    JMMN