Part Number: DS90UB949-Q1EVM
Other Parts Discussed in Thread: ALP
Hello. I'm working with the DS90UB949-Q1EVM to test a DES product that includes basically the images source. So, I'm using the Pattern Generator of the Analog Launch PAD that have 16 Patterns pre-loaded but I would like to load my own image (e.g. a chessboard with predefined pixel size squares). Could you explain if I can do it? is there a manual to config the custom image? can I change it "on-the-fly" in order to verify several images? Additional, how can I configure frequency and keep it (e.g. 50 or 60 Hz)? Thanks in advance for your support.