Part Number: SN65LVDS047
Other Parts Discussed in Thread: SN65LVDS048A, DS100BR410, SN65LVDS31, SN65LVDS390, SN65LVDS391, DS25BR440
Hi,
I would like to ask you to give me your advice about following system.
Q1) Is it possible to send data from board1 to board2 via board2 by LVDS? (around 30cm)
For example, "SN65LVDS047 + SN65LVDS048A" can do it?
Q2) Or should I use "repeater" on board2?
For example, "SN65LVDS047 - DS100BR410 - SN65LVDS048A" is better system?
The specification is as below.
CH number : 4ch
Data rates : over 480Mbps
skew : as small as possible
Will you advise me how to make the system and recommend me appropriate solution, if possible?
And will you also tell me something material to explain LVDS solution?
Thank you very much for your support.
Best Regards,