This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB954-Q1EVM: Internal Eye monitor setting

Part Number: DS90UB954-Q1EVM


Hi team,

We use 953-954 in synchronous clock mode.

I connect the board we made to a PC and perform system verification using Margin Analysis with TI GUI.

When the communication rate was 4 Gbps, there was not much margin, so I set the back channel to 25 Mbps as a trial and tried again to 2 Gbps.

Then, the margin was expanded, but the result was that all PASS was done with the one with the larger strobe position l like a 14, 13 and 12.

I was thinking that both fast and slow strobe positions would fail, so I'm not sure if it's correct that all the slow ones pass.

Is there a register that needs to be changed to perform Margin analysis when the back channel is dropped to 25Mbps and it is set to 2Gbps in the 4 Gbps synchronous clock mode setting?

Best regards,

Tomoaki Yoshida

  • Hi Yoshida-san,

    Could you provide the screenshots of the results so I can understand it better?

    Margin analysis test is done the same way regardless of the forward channel rate. There's no additional registers you need to program.

    Best,

    Jiashow