Part Number: SN75DP130
Hello support team.
Datasheet of SN75DP130 says the VID as Peak-to-peak input differential voltage at RBR, HBR, HBR2 for MAIN LINK TERMINALS on SN75DP130 is 0.3Vp-p min and 1.4Vp-p.
However, VRX-DIFFp-p for RBR in the VESA DisplayPort Standard is 40mV then my customer is getting a confusion. Is this means SN75DP130 doesn’t support the VESA DisplayPort Standard? Please clarify how the customer need to think the allowable input level on SN75DP130. The customer said the actual voltage is a little bit less than 0.3Vp-p but not close to 40mVp-p. Of course the customer try to check the eye opening to follow the VESA DisplayPort Standard.
Best regards,
Izumi Maruyama