Part Number: DS90UB941AS-Q1
Other Parts Discussed in Thread: DS90UH948-Q1
Hi team,
I have some problems using the DS90UB941 with the DS90UH948.
The interface chip model of the display is DS90UH948-Q1, without touch, and no audio. The resolution of the display is 1280*720
Whether only one DSI input can satisfy the requirement of video transmission on display screen.
For the use of two configuration pins, please help check if it should be configured as Continuous DSI Clock Mode.
For the suggestion of layout, please also help.
THANKS.