Part Number: DS110DF1610
Tool/software: WEBENCH® Design Tools
We use ds110df1610 to make a layer of wire card.The test connection is as the pic.
When the port is connected, it is found that the first port and the second port of the switch cannot link, but the corresponding channel obtained from the line card can check the port and can be locked.
The initialization of the chip was done according to the instructions of the chip, and now the configured rate is standard Ethernet, which can be locked for 1G and 10G, but not for 2.5g and 5G.
We adjusted the vod according to the table in the datasheet 6.3.1.7.1, but the switch still could not link.
Even if we do not turn on the cross point switch function (adjust the fiber connection, the module is also a dual fiber module), the phenomenon is the same, the switch still cannot link.
Please help to analyze the issue.
Best regards.