Hello,
My company using DS90UB941AS-Q1.for IVI module
Connected display has various screen resolution 1080, 720 and other also.
With 1 LVDS differential pair what is maximum screen resolution?
Best regards,
JaeHoon
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
My company using DS90UB941AS-Q1.for IVI module
Connected display has various screen resolution 1080, 720 and other also.
With 1 LVDS differential pair what is maximum screen resolution?
Best regards,
JaeHoon
Hello JaeHoon,
Important to know that this device supports for a single link a PCLK up to 105MHz.
You can calculate your required resolution using this formula:
PCLK = Htot x Vtot x Fps x blanking
Thanks for your feedback.
I made calculation sheet as below. (I don't know actual spec of display)
Screen resolution |
Frame rate |
Blanking period factor |
H-Res | V-Res | Blanking period factor |
Required Pixel clock |
Bits per pixel (color depth) | Data Rate | Required LVDS pair |
Hz | Mhz | bpp | Gbps | ||||||
800x480 | 60 | 10% blanking | 800 | 480 | 1.1 | 25 | 24 | 0.594 | 1 Pair |
1280x720 | 60 | 10% blanking | 1280 | 720 | 1.1 | 61 | 24 | 1.4256 | 1 Pair |
1336x768 | 60 | 10% blanking | 1336 | 768 | 1.1 | 68 | 24 | 1.587168 | 2 Pair |
1329x802 | 60 | 10% blanking | 1329 | 802 | 1.1 | 70 | 24 | 1.648749 | 2 Pair |
1440x900 | 60 | 10% blanking | 1440 | 900 | 1.1 | 86 | 24 | 2.00475 | 2 Pair |
1600x900 | 60 | 10% blanking | 1600 | 900 | 1.1 | 95 | 24 | 2.2275 | 2 Pair |
1680x1050 | 60 | 10% blanking | 1680 | 1050 | 1.1 | 116 | 24 | 2.728688 | 2 Pair |
1920x720 | 60 | 10% blanking | 1920 | 720 | 1.1 | 91 | 24 | 2.1384 | 2 Pair |
1920x1080 | 60 | 10% blanking | 1920 | 1080 | 1.1 | 137 | 24 | 3.2076 | 3 or 4 pair |
1920x1200 | 60 | 10% blanking | 1920 | 1200 | 1.1 | 152 | 24 | 3.564 | 3 or 4 pair |
1280x720, 60Hz 24bpp will work with 1 LVDS pair.
From 1336x768 60Hz 24bpp need lat least 2 LVDS pair due to max data rate of lane
From 1920x1080 60Hz 24bpp need 3 or 4 lane due to max data rate of lane
If my calculation and assumption is not correct, please let me know it.