Part Number: TCA9555
Other Parts Discussed in Thread: IO-EXPANDER-EVM, TCA8418E, TCA8418
I am using a TCA9555 as one of the slave devices on my I2C bus.
It has been set up on the IO-EXPANDER-EVM by removing the part that it comes populated with. I am trying to generate an interrupt on pin 1 of the TCA9555 using the breakout pin provided on the EVM.
To do this, I have built a temporary circuit on a breadboard, which pulls up the breakout pin to +5V using a 2k Ohm pullup resistor.
I configured port 0 as an input (writing all 1s to the Config0 register). I changed the jumper position on J12 from out to IN.
I am polling the IO Expander port 0 once a second. Should a button press on S3 using this configuration assert the INT pin low?