Part Number: TCAN332
Application note SLLA279A provides a formula for spacing CAN nodes to get reliable transmission. The article seems to indicate that this would occur if you had a really long bus length (as in the example provided), but the resultant equation for CAN node spacing is independent of the overall bus length. The equation d> CL/0.98C meters, where d=node spacing, C is in pf/m and CL is pf. Is there some additional condition for this to be applicable? As it stands, it appears that if the nodes were separated by 1m vs. 100m, it wouldn't matter => the same equation would apply.