Part Number: DP83825I
Hi, Team,
We have questions for the pin function.
1. Qestion for "Reset:1, PD; Active: O" pin.
-Are these pin Pulled-dwn during reset?
-Are there pin becomes Hz after reset?
-Is the resister value typ: 19kohm?
2. Qestion for "Active:I, PD/Active:I" pin.
-Are inside PD/PU of these pin active during the IC is working?
Best Regards,
Satoshi Yone