Part Number: TMDS181
Hi Team,
We want to do both lane swap and polarity swap on the input and as the datasheet mentions that polarity swap doesn't work in redriver mode, we want to make sure that the device works in retimer mode all the time. I found that this can be done by setting bit [1:0] of Register 0Ah to “11”, however, since we are going to use pin strap to configure this device, is there an alternate way to accomplish this?
Thanks!
Roy Hsu