Part Number: TCAN4550EVM
Other Parts Discussed in Thread: TCAN4550, TCAN1043
Hi,
I am attempting to communicate in the following fashion: MSP432 -> TCAN4550EVM -> TCAN4550EVM -> MSP432.
The MSP432's have 3 wire SPI master code on them.
I am wondering what the default test mode is for the TCAN4550, from what I can tell it seems I am in a loop back mode.
1.) Which test mode should I use for my evaluation case? How do I switch to it using the EVM?
2.) Is there any sample code for a similar functionality?
3.) I have also noticed that at my SDO pin on both TCAN4550s, the voltage is at most 800mV, while SDI (from the MSP432) is around 3.3V. Note that I have VIO set to 3.3V on the EVM. Is this expected?
I appreciate any clarity or comments you may have on my set up, and please ask questions if you have them. Also, if there is anything I should be aware of/look out for, please advise.
Best,
Grant